12/30/2007 4:56 PM | |||
Joined: 1/7/2006 Last visit: 3/9/2025 Posts: 2705 Rating:
|
Dear Nawaz, You are on the right way, you need a Modbus RTU Master package, to save some money you could buy the
Then you need to install the package PtP Param V5.1 incl. SP8(it for free) and you have also to install Modbus Master(also no payment) software to parametize the CP341. If the data isn't that much you could also use a ET200S 1SI module (6ES7138-4DF11-0AB0 USS Serial Interface Module, there you didn't need a copy license, but the data that you could send/receive is less in the same time as for a CP341. But when you have only one slave then that is possible... SeeSerial Interface Module ET 200S 1SIfor more information about the 1SI module for the ET 200S. Also there are some examples for this module: Function Blocks, Examples and User Manuals for the ET200S 1SI Serial Interface |
||
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|||
5/9/2016 2:12 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by vrk is split to a separate thread with the subject Communication between 3WL breaker with COM16 module as Modbus slave & S7-1500 CPU 1511-1pn with 1SI MODBUS MASTER. Best regards |
Follow us on