8/26/2014 6:59 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of a not registerted user
|
8/26/2014 12:26 PM | |
Posts: 168 Rating:
|
The Unisab III controller is equipped with a Profibus communication port. The Unisab II can if it's an early version be upgraded with a Profibus communication port, the later versions of the Unisab II was shipped with the upgrade. The built in RS-485/422 port of the Unisab II is only for use with their dedicated slave system. You can find more information here: http://www.sabroe.com/en/products/controls/ Their support is outstanding, I found them to be very helpful when I had to implement a Profibus communication to a PLC system. I was supplied with ready to use function blocks for both Siemens 300 and Mitsubishi Q and FX system. Edit: I found the GSD files for Unisab II and the program examples for Step 7 if anyone is interested. |
Last edited by: Bryll at: 8/26/2014 2:01 PM |
|
This contribution was helpful to
1 thankful Users |
6/3/2017 9:44 AM | |
Posts: 168 Rating:
|
As I now and then are asked to send the Sabroe GSD files for the Unisab II controller and examples. GSD files attached as a start. Unfortunately are the examples to large to upload here. They are made in Step 7 classic. AttachmentUnisab II GSD Files.zip (704 Downloads) |
This contribution was helpful to
2 thankful Users |
6/3/2017 9:49 AM | |
Posts: 168 Rating:
|
Documentation examples attached AttachmentDocumentation_Examples_siemens.zip (680 Downloads) |
This contribution was helpful to
1 thankful Users |
6/3/2017 9:52 AM | |
Posts: 168 Rating:
|
Program examples attached. Do not ask me about the examples, they are not mine, I got them from York. Attachmentprogram_example_Siemens.zip (673 Downloads) |
This contribution was helpful to
3 thankful Users |
3/27/2020 9:22 PM | |
Joined: 3/5/2008 Last visit: 9/26/2023 Posts: 12 Rating:
|
Hello, Can you please share files for Unisab III. Share files with wetransfer.com |
Follow us on