9/7/2013 8:48 AM | |
Posts: 1 Rating:
|
Dear All, Please find attached documents and below architecture. We wanted to do the data exchange between S7 300 & S7 400 H system. We are facing some problem in that communication. Please give me your inputs and kindly clarify the below questions. My Project 1(s7 -300) needs to do the data exchange wiht Project 2 (s7-400 H) system. 1. 1.Whichever the connection we use, is that required to do Net pro configuration on My partner PLC as well ( S7 400 H)? Please let me know, based on that I will have to confirm to my client as well. Ø With that above configuration when I was trying to create S7 connection , it was not able to create with that CP 343-1 Lean. For testing purpose I have changed my CP to CP343-1 NOT Lean then I was able to create S7 connection. Which means CP343-1 lean will not Support S7 connection. Please let know is that correct? Ø Since, both stations are under different project, while creating the S7 connections, I should select “Unspecified” for the partner side. Is that correct? Ø Even though The S7 400 H station (Partner) is under different project, still I have to add my partner Hardware station under my project. Is that correct? After I modify the Net Pro Configuration, when I download to my (PLC s7 300 ), will it get affect my partner PLC (S7 400 H ) because I have add and assign IP address for 400 H station as well under my project Th Thank you very much your help in Advance. B Best Regards, Sampath AttachmentArchitecture.pdf (234 Downloads) |
Follow us on