4/24/2012 12:48 PM | |
Posts: 21 Rating:
|
Hi, I have one question. I need to make connection over ethernet between 2 CPUs S7-400 and S7-300. I can edit whole project on S7-400 but cannot change hw-config on 2nd CPU S7-300. I will exchange 2 data blocks. One will be readed from S7-300 and 2nd should be writen to S7-300. Can someone give me advice how can I do this? With AG_SEND and AG_RECV is this possible? Here faq for this connection http://support.automation.siemens.com/US/llisapi.dll?func=cslib.csinfo&objId=22792404&nodeid0=10806025&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=US |
Last edited by: lazik at: 4/24/2012 12:50 PM |
|
4/24/2012 1:07 PM | |
Joined: 12/1/2009 Last visit: 2/9/2025 Posts: 672 Rating:
|
Dear lazik, |
Give us your feedback and show us your respect! |
|
4/24/2012 1:21 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello lazik, You need to modified the Backup on the S7-300 Side, because you need to defined the Connection with Other Side (S7-400 PLC or unspecified). |
Last edited by: Ammy at: 4/24/2012 1:24 PMAmmy |
|
4/24/2012 3:54 PM | |
Joined: 4/30/2007 Last visit: 3/9/2023 Posts: 231 Rating:
|
Hello lazik, one important thing you didn’t mention, if you are planning to use the integrated PN interface or a IE CP for each plc. In case of using CP’s you need to create the network connections using NetPro otherwise not. Moreover this also affects the selections of the communications blocks… |
Follow us on