Industry Online Support
Technical Forum
6/24/2012 11:49 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, Both systems you mention are S7 systems, there is no reason no to useS7 connections. But the topic is to large to be handled in a few sentences. See the manual http://support.automation.siemens.com/WW/view/en/60458386, chapter 14.5 "Communications via S7 connections". These S7 connections can be run in a one sided mode (chapter 14.5.1), in a redundant mode (chapter 14.5.2) |
Best regards |
|
Follow us on