7/30/2019 5:30 AM | |
Joined: 3/30/2019 Last visit: 3/9/2024 Posts: 3 Rating:
|
Hi Murof Thanks for taking the time. There are no errors, actually. I'm faced with some dead ends.. so to speak. Tried searching the manuals.. in vain. I'm using TIA portal V15. My KTP700 DP Image version: 15.00. CPU: 1214C and CM1243-5. I'm directly connected to the HMI from CM1243-5 via profibus cable. The CPU is connected to a router and I'm able get connected to the CPU- no problem!. I'm using a PC/Laptop,(no communication processor what so ever??) trying to download to the HMI. I've some screenshots.. On the profibus connectors, I'm terminated to the 'in' side on both connectors with the switch in on position. Appreciate the help.. thanks. Attachmentscreen_shot2_siemens_forum.pdf (87 Downloads) |
7/30/2019 5:32 AM | |
Joined: 3/30/2019 Last visit: 3/9/2024 Posts: 3 Rating:
|
Hey, Thanks. I've replied to Murof. Appreciate it. |
7/30/2019 8:53 AM | |
Joined: 8/3/2009 Last visit: 3/21/2025 Posts: 15056 Rating:
|
Hello I think now I understand, you want to do a Project transfer over routing (Ethernet -> Profibus). In This case (the Basic Panels 2nd Generation can do S7 routing Transfer in the newer TIA Versions) -> you have to create a network on the open Ethernet Port in TIA Portal. Then you open the Extended Download and then you can select the Network you are wanting to load over. https://support.industry.siemens.com/cs/ww/en/view/90528617 If I´m wrong with your usecase then you have to give me/us a new hint ;-) Bye Murof |
Last edited by: Murof at: 07/30/2019 08:54:19If this Information really helps, you could use the Rate function |
|
Follow us on