10/10/2009 3:20 PM | |
Posts: 9 Rating: (0) |
Dear Zoax; Please let me know which types of Telemecanique CPU's you have (PL7 or unity CPU) and Siemens CPU in order to give you the best solution. Regardes |
10/14/2009 4:46 PM | |
Posts: 21 Rating: (0) |
Dear J_Bell, thanks for you reply. Which communication block do you advise me to use in the Siemens PLC ? Best regards, Zoax |
10/15/2009 1:04 PM | |
Posts: 5822 Rating: (412)
|
Hello, I think you will need the FC 5 / FC 6 (AG_SEND / AG_RECV) from the SIMATIC NET Library for the CP and its TCP/IP Connection. Best regards J_Bell |
10/15/2009 3:58 PM | |
Posts: 21 Rating: (0) |
Hello J_Bell, thanks for your reply. I thought use TSend/TRecv. Can I use this function blocks ? Could you confirm that I have to realize the following procedure in NetPro in order to establish a tcp/ip communication ? 1. Add a other station. 2. Add a Industrial Ethernet Interface to this station. 3. Define the IP address of this interface 4. Add a TCP connection between the Siemens station and the other station. Thanks, Zoax |
10/15/2009 4:15 PM | |
Posts: 5822 Rating: (412)
|
Hello, the point is, if you use a CPU PN interface to do the TCP/IP Connection than you use TCON, TSEND, TRECV or TCLOSE. |
Follow us on