4/15/2009 8:48 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Hi, There is only possibility to write your own application on linux system to sommunicate to S7 controllers. There is Simatic.NET OPC server for linux. I didn't try it, but hope it will have some good manuals and examples. For example look here http://support.automation.siemens.com/WW/view/en/10806092/130000 |
Best regards, |
|
11/12/2009 4:48 PM | |
Posts: 1 Rating: (0) |
I tried to install Step 7 and run through WINE on Linux. First prompted message during installation "requires Internet Explorer". That's when I gave up. |
11/12/2009 9:27 PM | |
Posts: 1 Rating: (0) |
Look this: http://pvbrowser.org/pvbrowser/index.php I use that software on linux. |
1/29/2014 8:16 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hello! Yes, communication with S7 CPUs is possible under Linux. You can usethislibrary. Should work for S7-200, 300, 400 CPUs BR, olloy
|
10/31/2014 12:31 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! In this case you can write your program in Step7 undex virtual machine, thin just copu the blocks and download them to CPU withSnap7library, which works under Ubuntu as well. |
10/31/2014 3:44 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Argh, I didnt notice MPI. Sorry) |
Follow us on