10/3/2017 10:04 AM | |
Posts: 3 Rating: (0) |
Hello there. I am working on an automated coffee machine in the Mechatronics laboratory at the tshwane university of technology.Someone please help with the configurations of the two CP's. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/4/2017 8:20:29 AMNew subject after splitting |
|
10/4/2017 10:30 AM | |
Posts: 1368 Rating: (126) |
Hello, the S7-200 supports only Client-Server communication. Means: one S7-200 is Server, the other is Client. In this document, there is shown hwo to communicate between S7-200 (client/Server) to a S7-300 (server/client). For you, only the part "Configuration of S7-200 as Client" and "Configuration of S7-200 as Server" is interesting. https://support.industry.siemens.com/cs/ww/de/view/17369594 Perhaps it helps you, finding the problem... |
This contribution was helpful to1 thankful Users |
10/19/2017 6:50 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by watibe is split to a separate thread with the subject Do you have a link on communication between two scalances W?. Best regards |