6/4/2020 9:46 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello benzlpc you can use the same HMI Project on two WinCC Advnaced RT Stations but you have to set the IP Address in the Project before loading to the second station. (Of course you have to use unique iP addresses). -> where exactly do you need help? If you are not sure how to set up a common TCPIP Connection the look at this basic FAQ: https://support.industry.siemens.com/cs/de/en/view/89852595 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
6/4/2020 11:44 PM | |
Joined: 6/4/2020 Last visit: 11/20/2024 Posts: 4 Rating:
|
thank you frink |
6/5/2020 4:42 PM | |
Joined: 6/4/2020 Last visit: 11/20/2024 Posts: 4 Rating:
|
thank you very much frink |
Follow us on