Industry Online Support
Technical Forum
2/28/2008 2:29 PM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hi import-user-1, By default it is not possible to use S7-protocol suite in WinCC to communicate with s7-200 plc. -------------------- (1) OPC -------------------- - optional you can use the opc-server "pc-access" for the s7-200 plc. http://support.automation.siemens.com/WW/view/en/21915573 -------------------- (2) MODBUS and seriel interface card (RS232C) -------------------- -may be you can use modbus protocoll on seriell interface (com) on pc. ==> please refer attachment, this document was written for wincc V5.1; In earlier versions of wincc, wincc was delivered with modbus-driver by default: - "Modbus Protocol Suite.Chn" - "Modbus Serial.CHN" AttachmentSEC_0330_s22b_s7200_wincc_modbus_DOKU_v10_e.pdf (52 Downloads) |