Industry Online Support
Technical Forum
10/7/2008 2:20 PM | |
Posts: 487 Rating: (45) |
I do not think there is any thing special just because it is a telephone line.(Correct me if I am wrong) excepet it is going to be slow.One you are connected, you are not changing any communication protocol just changing the medium. So the onyl extra settings should be your dial-up settings.Make sure our DCOM settings are done properly. www.opcfoundation.org > Downloads > White Papers > Using OPC via DCOM with Windows XP Service Pack 2. |
10/7/2008 6:52 PM | |
Posts: 8 Rating: (0) |
Thanks JMJ for your response, i will work on this & get back soon. |
10/17/2008 12:06 AM | |
Posts: 5822 Rating: (412)
|
Hello, I wonder, have you done any test already? I would really appreciate to know more about your progress. J_Bell |
Follow us on