4/20/2017 10:45 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, sry, can you tell us how your PC RT change Ethernet to MPI, simply sry I can't imagine still this conversion, probably you've forget tell us using of some adapter/card???? |
Last edited by: Duris_I at: 4/20/2017 10:45:46 AMWith best regards... |
|
4/20/2017 12:07 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello Kanuzac in your WinCC Advanced RT Project you have an Editor "Connections". Look here at the Settings of your PLC Connection. There is an AccessPoint. In the most cases there is the Value "S7ONLINE". On your Runtime PC there is at the Windows control Panel the settings at "SetPGPC Settings" look if there is your MPI Adapter or communication Processor set for the AccessPoint S7ONLINE (Please note that you see "SetPGPC Settings" in windows control Panel only if you set the view to Small or large Icons) Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/25/2017 12:02 PM | |
Posts: 72 Rating:
|
Dear Expert, Now i test my Program with Wincc Flexible ( HMI program) and i write PLC (CPU313C) Program in tia portal . I set the Set PG/PC is S7online/ PCAdapter usb A2( MPI ) , and i can control PLC via HMI (Wincc Flexible). But in Tia portal , I choose PC Station (Wincc RT) , the problem is that the IE Communication is Profinet so i cannot make a connection with PLC. Do some one give me an advice in this case ? Thank you so much |
Follow us on