3/19/2010 9:28 AM | |
Joined: 10/7/2005 Last visit: 4/23/2025 Posts: 3047 Rating:
|
Hello Void Ican't tell you exactly what the problem is,I can tell you though that and AG_SEND error of 80C3 means: "The resources (memory) of the CPU are temporarily occupied" and you can find more hopefully helpful infoat the link below: What points do you need to remember when calling communication blocks FC5/50 and FC6/60 in the STEP 7 user program of the CPU? Bear in mind too that- owing to the nature ofa H-System - a H CPU does "loose" part of its communication performance through the synchronization that isrequired between the CPU's and the link below has more on this: Increasing the CPU load for a data length of greater than 240 bytes in the case of Send/Receive communication with Industrial Ethernet CPs I hope this helps |
Cheers |
|
3/20/2010 2:35 PM | |
Posts: 4 Rating:
|
Thanks a lot. I solves this problem by calling it 1 second one time. |
This contribution was helpful to
1 thankful Users |
Follow us on