8/20/2014 1:41 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
Try the latest update for V13, update 3 (I think). Also, since the error says to contact Siemens support, please do so via Support Request |
science guy |
|
10/3/2014 4:15 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
Please refer to the simulation software restrictions. If for example you are using the built in web server, the documentation I read said the web server is not available during simulation. Perhaps there is something about the problem you are having as something not supported. If it says it is supported and it does not work and you have the recommended or suggested amount of RAM available and are not using it to run say outlook, web browser, instant messaging, notepad, and a host of other processes that steal resources and memory from Portal, then submit a Support Requestto alert them of the problem. Archive and submit your project, the windows version, RAM, and let them reproduce the problem. If the problem goes away by selected the default language (Deutsch, or maybe English), then tell them that as well. If you have a local distributor with Siemens hardware for mini courses and technical hands-on, maybe you can visit them or they can bring it to you for a short term loan, you can try out your logic using their borrowed hardware. |
science guy |
|
Follow us on