11/25/2017 6:55 AM | |
Joined: 7/1/2017 Last visit: 8/6/2024 Posts: 1 Rating:
|
Hello sir, Please help with communication for S7-1200 and S7-300 PLC using get and put instruction.please tell me about its connection in TIA-V13 And so its properties. Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/27/2017 11:12:38 AMNew subject after splitting |
|
11/25/2017 8:26 AM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, you can start here with some useful infos: S7 PUT GET |
With best regards... |
|
11/27/2017 2:31 PM | |
Joined: 7/9/2015 Last visit: 3/18/2025 Posts: 4200 Rating:
|
Hi, here are some examples: How do you configure and program an S7 connection and the PUT and GET communication instructions for data transfer between two S7-1500 CPUs?or How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?Regards, Towome |
|
|
This contribution was helpful to
1 thankful Users |
11/28/2017 10:39 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi PARTH_PDSL, There´s a FAQ with exact this combination: hope this helps, regards, |
FCK WAR! |
|
Follow us on