9/17/2008 7:44 PM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
Hi Pravin The Guide for Configuration of CP341 as RTU Master attached herewith. Modbus Master Modbus Slave AttachmentModbus_master_e[1].pdf (335 Downloads) |
Last edited by: Deeps at: 9/17/2008 7:49 PM |
|
9/17/2008 7:50 PM | |
Joined: 9/27/2006 Last visit: 3/16/2025 Posts: 12344 Rating:
|
Hello Pravin; First here are the manuals for the loadanble drivers, Modbus RTU Master and Modbus RTU slave: http://support.automation.siemens.com/WW/view/en/1220184 http://support.automation.siemens.com/WW/view/en/1218007 Also look at the following FAQ for Modbus slaves on the CP 341: http://support.automation.siemens.com/WW/view/en/18865330 You will need to buy the dongle for the CP 341, and download thew PTP parametrization package for PTP communications, that will allow you to set the parameters for Modbus comms on the CP 341. http://support.automation.siemens.com/WW/view/en/27013524 I will look for information in the setup of USS on the CP340, and I am sure you will have other chime in also. But could I ask you why you choose USS, when Profibus-DP is much faster and robust? Question of cost? The CP340's cost must figure in somewhere in the price evaluation. Just curious. Hope this helps, Daniel Chartier |
Follow us on