5/24/2011 9:08 AM | |
Posts: 23 Rating:
|
What is the appropriate method of communicating an S7 400H controller station with PCS7.... 1)Communication with an Ethernet CP S7 Communication Send-Receive communication 2)OPC The configuration of the S7 400H station is attached herewith AttachmentSystem configuration.zip (151 Downloads) |
5/24/2011 11:28 AM | |
Posts: 212 Rating:
|
hi, You have mentiond PCS7 in thread and system configuratiion shows MP. Please clarify what exactly is needed. use this thread for answers if you need PCS7 /tf/WW/en/Posts/33797 |
5/24/2011 1:53 PM | |
Posts: 23 Rating:
|
Hi , This configuration of S7 400H Controllers with MP377 needs to be communicated with PCS7 |
5/26/2011 6:04 AM | |
Posts: 212 Rating:
|
hi Do you mean to say in your configuration S7400 H and PCS7 stations are available and along with that you have Mp377 also. Ok. you can use MP 377 to communicate with S7 400H over ethernet or Profibus. Connection with profibus is as follows. 1. http://support.automation.siemens.com/WW/view/en/13595393. For downloading gsd file for the same refer attached link http://support.automation.siemens.com/WW/view/en/29339779 You cant connect HMI over Y-Link. I could find a manual which covers all types of connection please find @ http://support.automation.siemens.com/WW/view/en/23842653 post your comments |
5/27/2011 8:45 AM | |
Posts: 23 Rating:
|
I guess I was not clear in presenting my query intially.Let me do it now.... Also find attached the configuration for reference. I have completed Engineering with S7400H controllers with MP377(Communicated on Ethernet)-Unit Control Panel.Now the client is having PCS7 station which requires communication with this unit control panel package.what would be the options Attachmentconf.zip (107 Downloads) |
Last edited by: Sindhu@keas at: 5/27/2011 8:45 AM |
|
5/27/2011 9:03 AM | |
Posts: 212 Rating:
|
hi, what I feel is the configuration is still presented incorrectly. it should be like attached one hence for ethernet method of communication is explained @ http://support.automation.siemens.com/WW/view/en/23842653 Attachmentact config.pdf (101 Downloads) |
Last edited by: ABN at: 5/27/2011 9:04 AM |
|
Follow us on