3/11/2016 8:55 AM | |
Posts: 767 Rating:
|
Dear All, I would like to know that, is it possible to communicate S7 300 & ABB Cluster Modem CI-840. Please help. |
3/12/2016 2:24 PM | |
Joined: 9/27/2006 Last visit: 3/27/2025 Posts: 12344 Rating:
|
Hello rocket; With a simple search, you also could have found such a document from ABB, with the following information:
Communication
S800 I/O uses Advant Fieldbus 100 or PROFIBUS as an external communication interface and ModuleBus as an internal communication link between clusters and their I/O modules.
Fieldbus Communication Interface
A Fieldbus Communication Interface module is used as communication interface to connect S800 I/O modules to the fieldbus.
There are five different FCI modules:
• CI801 for PROFIBUS-DPV1
• CI810 for Advant Fieldbus 100, with or without media redundancy
• CI820 for Advant Fieldbus 100 fully redundant communication
• CI830 for PROFIBUS-DP
• CI840 for PROFIBUS-DPV1 fully redundant communication To locate the CI840 gsd file find out if (and how) you can use it on a non-redundant Profibus link (such as the one provided by a standard Siemens PLC, except for a S7-400H system) you would have to search further or ask ABB directly. Hope this helps, Daniel Chartier Edit: you can find the CI840 gsd file at the bottom o this download page from ABB: http://www.abb.com/abblibrary/DownloadCenter/?showresultstab=true&QueryText=gsd
D.C. |
Last edited by: dchartier at: 3/12/2016 2:25:11 PMLast edited by: dchartier at: 3/12/2016 3:54:37 PM |
|
This contribution was helpful to
1 thankful Users |
3/14/2016 6:08 AM | |
Posts: 767 Rating:
|
Thanks for the reply.. |
Follow us on