11/22/2018 3:17 PM | |
Posts: 13 Rating:
|
Hello, I'm facing the same situation but with V13. I have a simple project on Wincc7.4, which is animate a red ball, when I have the bit activated it turn's green, and I'm trying to simulate him on TIA PORTAL V13 using the S7-PLCSIM. The PLC that i am using is a S7-1500 as shown on the image. The TIA PORTAL programm is working correctly with s7-PLCSIM, but PLCSIM is not working together with wincc7.4. In Tag Management I have the configurations that you can see on the images, and in PG/PC settings i have these. What I need more? It's shows me green on Tag Management but it doesn't work. Thank you, wainting for your answer João Martins ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/24/2018 8:09:11 PMNew subject after splitting Last edited by: Jen_Moderator at: 11/24/2018 8:09:52 PMEdited headline. |
|
11/29/2018 10:41 AM | |
Posts: 13 Rating:
|
Hello sorry for the late answer. I solved the problem. The simulator and the PLCSIM didn't had the same IP address. |
Follow us on