8/23/2016 9:37 AM | |
Posts: 26 Rating:
|
Here are accesible devices in Profinet. The device name of IM151-3 is the same as in the TIA project. |
8/23/2016 11:19 AM | |
Posts: 26 Rating:
|
Dear Christoph, I downloaded the al rebuilded HW Config (PLC_1 -> right click -> Compile hardware (rebuild all) then PLC_1 -> right click ->Download to device -> Hardware configuration). Actually I do this sequence of actions every time. But by going online I still receive the warning message: "Going online: the HW configuration of the PLC_1 was changed but it was not compiled and loaded yet. The shown diagnostics is possibly inconsistent or wrong". Also I compared online and offline configuration. But the message was "Offline/online comparison completed successfully. Result is saved in additional files". I don't know how to open comparision file in TIA, but I found in in project. I attached it as text file. AttachmentTopologicalDetection1.txt (215 Downloads) |
Follow us on