4/10/2017 1:18 AM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello narove; 1- FMS has been abandoned for a while now, in favour of Ethernet communications, since they operated at the same level (message-wide protocols) and Ethernet found favour in the industry. A few years back I saved a chapter of the NCM S7 for Profibus manual which describes different Profibus connections available on S7 CPs (DP master/s;lave, FDL, FMS), with sample design suggestions. Chapter 6 describes the essentials of communicating over FMS between 2 S7 CPUs. You will find it as an attachment, since I can't seem to locate a download link for that particular manual now . If I remember well, the most important aspect is to create a proper FMS variable, indexed, before attempting to exchange data. Follow the step-by-step example, pay attention to the definitions and the details and do not cut corners; that is how I started working with FMS . You should be alright. 2- Size of the maximum data exchange per job (you can create more jobs, call them sequencially) SIMATIC NET NCM S7 for PROFIBUS / FMS volume 2 On an FMS connection, the PROFIBUS CP can transmit an FMS protocol data unit (FMS PDU) with a maximum length of 241 bytes per job. Hope this helps, Daniel Chartier AttachmentCommunication over FMS connections.pdf (195 Downloads) |
Last edited by: dchartier at: 4/10/2017 1:24:28 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on