2/3/2018 8:39 AM | |
Posts: 11 Rating:
|
Dear Experts! Advice required S7300 CPU 2 DP 315 Master Slave Profibus.(2 CPU) In My application I have to send data from Master to slave and slave to master but I can only be able to send data from Master to slave only via Profibus Below attached program is running ok with 1- Profibus link ok 2-Data is receiving from master to slave non consistent and consistent data 3>4 Bytes Please advise 1- how to send data from slave to master Task Attempted: OB1 Use code for SFC 14-15 & SFC 20 for Slave in same way to transmit data to master but not got any result only master to slave side is working 2- Could we transfer real Float values from M-S /vice versa .Currently I have to do round first then move to Word or D-Word in Array DB. Thanks! AttachmentProfi_Te.zip (148 Downloads) |
2/3/2018 9:08 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, I suggest you to start with this FAQ is Master 400 and 300 slave but is the same. DP link between CPU 315-2DP (slave) and S7-400 (master) with ... |
Last edited by: Jen_Moderator at: 2/5/2018 11:16:41 AMOptimized link. |
|
2/3/2018 10:33 AM | |
Posts: 11 Rating:
|
Attachmentattachments.zip (130 Downloads) |
2/3/2018 11:36 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, there is some limitation with DP port of the CPU, you have to use I/O area and not DB to exchange data, for more information please have a look this thread below and in particular our expert dchartier: Two 315-2DP CPUs Profibus Master-Slave communication - Entries ... |
This contribution was helpful to
2 thankful Users |
2/10/2018 10:27 AM | |
Posts: 11 Rating:
|
Ok i'll try to optimize it.Thankful for your support |
This contribution was helpful to
1 thankful Users |
Follow us on