2/28/2013 12:39 AM | |
Posts: 4 Rating:
|
Does anyone knows how can I communicate some relays GE 650 with CP 341? I have no experience to do this. Thanks so much. |
2/28/2013 4:37 AM | |
Joined: 9/27/2006 Last visit: 3/20/2025 Posts: 12344 Rating:
|
Hello HarGui; Do you mean a F650 bay controller from GE? Such as this one: http://www.gedigitalenergy.com/products/manuals/f650/GEK-106310AA.pdf If this is the right relay, then the manual describes how to connect using Modbus RTU, which is supported by the CP 341. How much do you know about Modbus RTU? What do you know about the CP 341? How much do you know about the CP 341 as a Modbus RTU master? Are you going to need a RS-232 or a RS-485 interface? Hope this helps, Daniel Chartier |
8/24/2017 4:16 PM | |
Posts: 5 Rating:
|
Any updates on this? |
8/30/2017 9:08 PM | |
Joined: 9/27/2006 Last visit: 3/20/2025 Posts: 12344 Rating:
|
Hello Dusan; from the chapter on Modbus comms in this manual, it seems that the mapping of the Modbus registers is individually designed for each Ge F650 relay, and that they can be reached by standard Functions 3, 4 and 16, as any "normal" Modbus slave. Have a look at chapter 8 in this link: http://ftp.so-ups.ru/RZA/GeneralElectric/%C0%CD%C3%CB/manuals/f650/f650man-i.pdf See if you can obtain the Modbus mapping of your relay through the F650PC software, and if it really is located in addresses 3000x and 40000x. Hope this helps, Daniel Chartier |
Follow us on