5/7/2009 1:29 PM | |
Joined: 9/27/2006 Last visit: 1/15/2025 Posts: 12328 Rating: (2699) |
Hello Denis; You say that your problem is related to the TSAP number you have selected. In the link you provide, different TSAPs (Transport Service Access Points, an OSI tool for identifying the interconnections between the data layer and the transport layer of the ISO 7-layer communication model for Ethernet) are proposed depending whether the S7-200 is server or client, and the S7-300 is server or client. Look at the following discussion that we had here last month, especially at Helmut and J_Bell's explanation of the TSAPs used with PC-Access (an OPC server for the S7-200); it might explain some details: /tf/WW/en/Posts/26160 So please tell us how you have selected the server and the client in your application, how you have set them up in MicroWin and Netpro (Step 7), and then how the TSAPs required are not possible to write in. Then we might be able to sort the problem out with you. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/7/2009 1:33 PM |
|
5/8/2009 12:40 PM | |
Posts: 7 Rating: (0) |
If I have correctly understood that such ar the names:
"req"- M14.1 "nrd" - M14.4 "error" - M14.5 "status" - MW60 |
5/8/2009 12:59 PM | |
Posts: 7 Rating: (0) |
IP the address and TSAP to me founders of the project for S7-200 have told. It turns out, what something on S7-200 is made not how they speak? |
Follow us on