8/1/2015 9:24 PM | |
Posts: 1 Rating:
|
Dear Siwarexi, Thanks for your support. I have a question. do I need to connect a S7 PLC or E200 to adjust parameters of siwarex? because I have connected the siwarex to PC and opened the siwatool however, it fails all the time to activate communication. note: as i connected the siwarex to PC all the indication lamps are lit and stay like this. I don't know if it is supposed to be lit all the time of communication or not?
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 8/3/2015 9:46:50 AMNew subject after splitting |
|
8/4/2015 8:21 AM | |
Joined: 1/4/2007 Last visit: 9/22/2023 Posts: 1059 Rating:
|
Hello Hazemwaddah,
Helped the comment from ABenno?
If not: Which Siwarex module do you have?
Best regards
Siwarexi |
Follow us on