8/7/2008 11:46 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, With SFC 62 "CONTROL," you can query for S7-400 the status of a connection belonging to a local communication SFB instance. After calling the system function with the value 1 at control input EN_R, the current status of the connection belonging to the communication SFB instance selected with I_DB is queried. I_CONN OUTPUT BOOL I, Q, M, D, L Status of the corresponding connection, possible values: • 0: Connection down or notestablished• 1: Connection exists |
Last edited by: edr at: 8/7/2008 11:52 AMBest regards |
|
Follow us on