6/9/2010 7:17 PM | |
Posts: 19 Rating:
|
Hello, is it possible Ican communicate to a thrid party OPC server directly from PLC (S7-400H). It means an OPC client can be implemented using cp443-1? Regards, Shakil Splitted from I want to use plcsim with WinCC with OPC connection in S7-400H sample project. |
Last edited by: O_Moderator at: 6/10/2010 8:03 AMnew subject after splitting |
|
6/10/2010 8:04 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Threads closed, because question is already published in the following thread want to connect OPC server (third party) to S7-400 plc. Best regards O_Moderator |
Follow us on