Industry Online Support
Technical Forum
12/1/2008 8:45 AM | |
Joined: 4/6/2006 Last visit: 1/21/2019 Posts: 604 Rating:
|
Hello Genral, Ok. Then it seems to be a failure. Can you try the following FAQ? Why do no PROFINET components appear in the primary setup tool or in STEP 7 -Display Accessible Nodes-? http://support.automation.siemens.com/WW/view/en/23585653 If this doesn't work i would suggest to open a Service Request at the hotline. |
Best regards, |
|
12/1/2008 10:29 PM | |
Posts: 3 Rating:
|
Problem solved. I had "PROFINET IO RT-Protocol (LLDP)" installed but not "PROFINET IO RT-Protocol". Now with both installed the plc is recognised. Thanks mate |
Follow us on