3/8/2018 11:20 AM | |
Joined: 2/12/2018 Last visit: 11/26/2024 Posts: 224 Rating:
|
Hi I have a HMI (TP1200 Comfort) and a PLC (CPU 1513-1 PN) that I want to connect to a customers network so they can have Remote access using Sm@artServer. I have a LAN cable between PLC port x2 and HMI port x1, so that there is connection between them. Can I just connect my costumers network to PLC port x1 or HMI port x2, and then change the IP-address for both the PLC and HMI so it is the same as my customers network? As far as I can read, both the PLC and HMI have ethernet interface. Best regards |
Please don't forget to rate :) |
|
3/12/2018 11:46 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by Azkaban is split to a separate thread with the subject What is the difference between Industrial Ethernet (IE) and ProfiNet?. Best regards |
Follow us on