10/27/2008 7:43 PM | |
Posts: 433 Rating:
|
Hello romeo291, have a look at this link: OpenModbusTCP. I assume this is the functionality, which you want to realize... Tomcat |
10/27/2008 8:24 PM | |
Posts: 433 Rating:
|
Hello romeo291, for OpenModbusTCP you don't need any additional hardware - especially you don't need a serial CP (CP341) for a TCP communication... This product uses the functions AG_SEND and AG_RECV internal to send and receive datas to/from a third party communication partner. You can read/write holding registers and you can read input registers. Here you can download some documentations: FAQ + Download. Why do you want to "tinker" something when a complete solution is existing already? Tomcat |
Follow us on