Industry Online Support
Technical Forum
8/9/2007 4:14 PM | |
Posts: 6 Rating:
|
In the PG/PC Interface, there is no CP5611 that I can choose. So I went to add an interface, clicked on the the CP5611, but I could not install it? |
8/10/2007 11:46 AM | |
Joined: 4/24/2006 Last visit: 12/1/2023 Posts: 8596 Rating:
|
Hi, If you want to use OPC server to access data of CPU, it's possible. Please have a look at following Link: http://support.automation.siemens.com/WW/view/en/15364951 It's important to set PG/PC interface to PC internal. You make a configuration in NCM PC manager (CP5611 and OPC server). Also make a S7-connection in Netpro. To an unspecified partner with the profibus address of S7-300 CPU (Please pay attention to Address details) Make sure you download configuration and connection to PC. (PC internal) Then you can check with OPC scout. Hope this will help. Best regards, Wizard |
Follow us on