11/6/2013 3:14 PM | |
Posts: 1368 Rating:
|
Hello Iulian_84, if the barcode scanner is a profinet device, you can bind it on the profinet controller (S7-300) via GSDML file. Your barcode scanner will get input and output addresses for the status and control byte and for the user data. The meaning of the bytes you can see in the manual. Over this byte, the PLC and the barcode scanner communicate each other. Here you find an example with the code reading system MV440 and aPLC S7-300 http://support.automation.siemens.com/WW/view/de/56348738 Greetings, Pittiplatsch |
Follow us on