Industry Online Support
Technical Forum
1/26/2010 8:40 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating: (159) |
HI, When You installed the CP 341(Modbus Software CD) Software CD it will Installed the Sample project In the Sample Project Tab in the Open Project, This CD is come with Modbus Master or Slave Dongle. you can used the Same for your Application, Holding Resister is stating from 40000, you can used to send the data to the DCS & 30000 to Receive the Data From the DCS, in the Smae Project you will get the all the information related to Modbus, Manual For The Modbus Slave, http://support.automation.siemens.com/WW/view/en/1218007 Manual For The Modbus Master, http://support.automation.siemens.com/WW/view/en/1220184 |
Last edited by: Ammy at: 1/26/2010 8:48 PMAmmy |
|
Follow us on