7/13/2015 9:02 AM | |
Posts: 15 Rating: (0) |
Hi, In the previous systems, we used Profibus DP for communication between PLC and other system devices, and also TCP/IP for communication between PLC(S7-300) and IPC547E (WinCC). But now, at the same time, we must use IEC61850 TCP/IP for communication between PLC and Siprotecs (7SJ62). In brief, desired communication protocols between devices are in the following table; PLC <-> IPC(WinCC) àIndustrial Ethernet (TCP/IP) PLC <-> Siprotecs àIEC61850 IPC (DIGSI,SICAM etc.) <-> Siprotecs àIEC61850 PLC <-> Other system devices àProfibus DP Now, Is network structure in atthacted suitable? Which library license must be used for communication between PLC and Siprotecs? Best Regards, Emir, AttachmentNetwork Structure.pdf (273 Downloads) |
7/13/2015 10:52 AM | |
Posts: 15 Rating: (0) |
Sorry, It is wrong structure. My mistake. Right network structure is atthacted. AttachmentNetwork structure.pdf (343 Downloads) |
11/5/2015 9:28 AM | |
Joined: 8/21/2014 Last visit: 8/30/2024 Posts: 1006 Rating: (13) |
New question published by v.emir is split to a separate thread with the subject Communication with IEC61850 - ERROR output of COM block is high. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on