10/29/2010 2:39 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Thomas, The error descriptions for the error value shows that it is an internal error. Transfer the function to plc again and try it. Regards, Behnam www.sigmarocess.ca |
11/2/2010 1:26 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Thomas, There is a firmware update available for your CPU but there was nothing about Ethernet communication in it. How about creating a new code, just OB1 and call the function in it and see if any other error comes up? Regards, Behnam www.sigmaprocess.ca |
11/3/2010 8:46 AM | |
Joined: 10/7/2005 Last visit: 3/20/2025 Posts: 3042 Rating:
|
possible, but unlikely in my oponion dear Thomas_30. Your problem is indeed a bitstrange and I'd say you have done your "homework" very thoroughly. I suggest you raise a Support Request with Siemens and provide them with the gathered information (my money is on an "undocumented feature" of the firmware). Should you feel like doing more "homework" though, I think the following may be worthwhile testing: 1.) Assuming you use TCP, try "Ad-hoc" (LEN parameter 0) as well a fixed lenght mode(LEN parameter <>0) 2.) Try the other Ethernet port of theCPU(I know this shouldn't matter, but its a quick and easy test). 3.) Please check again the RET_VAL (your first entry says its 80F7 and the second says its807F). This is just to make sure you give Siemens the correct information, it is either way a "specific error code" that we can't determine further as TRCV uses SFC136 inside for which no help exists. That's all I can think of, good luck and please let us know about the outcome and/or feedback from the Support request. |
Last edited by: fritz at: 11/3/2010 8:49 AMCheers |
|
Follow us on