1/24/2018 1:47 PM | |
Posts: 4 Rating:
|
Hi, I am working as well in a communication with a Sick 2D laser Sensor LRS3600, What i am doing so far is to follow the example for "TCP native" and the related manuals (Open TCP Communication via industrial Ethernet). I cannot achieve that FB65 "TCON" connect with the sensor. The messages are always the same error code:7000. I generate the communication parameters with the wizard provided and changing the communication type to: "TCP Compatibility Mode" B#16#11. The CPU ia m using is the CPU317F V3.2 I have assigned to the sensor, for the ethernet comms, ID number=1, port 2112 to exchange data in binary, and IP address 10.0.0.190. On the other hand, the PLC is setup with IP address 10.0.0.11 and Id 2 (according to the hardware configuratuion, slot of the PN-IO in X2). I am completly stack, the communication is not even starting!! Please I would need help!! Thank you very much in advance, Kind Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/6/2018 12:35:33 PMNew subject after splitting |
|
2/2/2018 12:07 PM | |
Posts: 4 Rating:
|
Hi, Thank you very much for the answer, The part number is :(CPU317F-2 PN/DP) 6ES7317-2FK14-0AB0 Regards, |
Follow us on