Industry Online Support
Technical Forum
5/27/2008 9:21 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating:
|
Hi Supreame I think that you have Integrated the WinCC Project in the SIMATIC Manager, so I do not know ifyou set some parameters in the SIMATIC NetPro to establish the communication between the WinCC and the SIMATIC Manager or not . I have attached a file that will show you how to set these parameters (it is used to communicate the winCC with FH S7-400 so you can fit the parameters to achieve your demands) AttachmentNetPro[1].pdf (407 Downloads) |
Best Regards |
|
This contribution was helpful to
1 thankful Users |
Follow us on