10/3/2022 7:08 AM | |
Joined: 7/19/2022 Last visit: 1/24/2025 Posts: 433 Rating: (71) |
Hi RAJKIRAN; I have been able to add both in TIA Selection Tool and in principle there is no compatibility problem. I added the expansion module first and then the LOGO! Try it this way to see if it will let you. AttachmentScreenshots.zip (458 Downloads) |
Last edited by: JBS98 at: 10/03/2022 07:13:41If this Information really helps, you could use the Rate function |
|
10/3/2022 7:32 AM | |
Joined: 12/18/2014 Last visit: 1/25/2025 Posts: 34557 Rating: (4313)
|
All expansions module with 0BA2 at the end of the order number can you use with all 0BA8 LOGO!s. All expansions module with 0BA0 or 0BA1 at the end of the order number can you not use with all 0BA8 LOGO!s. 0BA8 LOGO!s: |
Last edited by: ixo65 at: 10/03/2022 07:32:49 |
|
Follow us on