Industry Online Support
Technical Forum
9/10/2014 7:32 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, maybe the DB1 is incompatible from 100U to 95U. Try to load the program without DB1 after clear PLC. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
Last edited by: sps-concept at: 9/10/2014 7:32 AM |
|
This contribution was helpful to1 thankful Users |
9/11/2014 11:56 PM | |
Posts: 3 Rating: (0) |
Both of you guys, thank you very much. I did exactly what sps-concept said, DB1 was the main and unique error. After remove DB1, the PLC started to restart, and back to run normaly. Thank you very much. I really apreciate the help. Regards. Michael Rodrigues.
Admin can close the topic. |
Follow us on