7/7/2011 8:06 AM | |
Posts: 30 Rating: (0) |
I have followed this video - http://www.youtube.com/watch?v=L9VFdP6eEu8 When i select the "Compile" menu item, nothing happens - the "compile wizard" dosent show. Do i needto do something more - set things up ? |
7/7/2011 10:14 AM | |
Posts: 30 Rating: (0) |
No clues ? This is a tough one for me. Tryed to reinstall Simatic 5.4 + SP 5, but no luck |
7/7/2011 11:52 AM | |
Posts: 30 Rating: (0) |
The video was not a solution -way to big... |
7/7/2011 1:18 PM | |
Posts: 30 Rating: (0) |
Hehe...The only video was in spanish - i'm dansih ;-) Compile AS ? - Hardware or something else ? |
Last edited by: Ulrik.V at: 7/7/2011 1:19 PM |
|
7/7/2011 3:31 PM | |
Posts: 30 Rating: (0) |
Thanks very much for all the help How do i check if if it is installed,and if not - how do i install ? |
7/8/2011 11:35 AM | |
Posts: 30 Rating: (0) |
This solved my problem - Thanks Per. There should be an error/information dialog when trying to compile without the tool installed |
6/19/2013 9:04 AM | |
Joined: 5/27/2011 Last visit: 1/31/2024 Posts: 22 Rating: (2) |
Hi Ulrik.V To do this, you must do the following steps. 1 - Install the software AS-OS Engineering WinCC software is available on CD. 2 - If you are on a computer OS and ES options open object must click on the OS and the software wincc properties allow activation on ES option enabled. Compile the file as it runs the video! Best Regards |
This contribution was helpful to1 thankful Users |