8/9/2018 5:41 PM | |
Joined: 11/1/2016 Last visit: 9/11/2020 Posts: 1 Rating:
|
Taking an older version of my project from V4.3 to V5.1. I have changed the device type from D425-2 V4.3 to D425-2 V5.1 and downloaded. Compliling in Scout I get an error: The Library 'LMCBasic.lib' does not support the device type 'D425-2 V5.1'. In Scout I've right clicked on the library -> Properties -> Technology Packages -> Upgrade, and it upgraded to V5.2 (even though I selected V5.1) This doesn't seem to have solved the problem, I still can't compile. What am I doing wrong? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/10/2018 10:03:23 AMNew subject after splitting |
|
Follow us on