Industry Online Support
Technical Forum
2/15/2012 6:29 PM | |
Posts: 11 Rating:
|
What cable do I use to download the pc to tp hmi 170b color? And which of the three port I use? |
2/15/2012 6:33 PM | |
Joined: 3/21/2006 Last visit: 2/6/2025 Posts: 10239 Rating:
|
Hello, Let's try it there: What transfer options are available in the various operator panels? SIMATIC HMI Touch Panel TP170 A, TP170 B Operator Panel OP170 B Best regards, Hristo Mihalev |
2/15/2012 8:11 PM | |
Posts: 11 Rating:
|
Hello These are the transfer options available in simatic panel TP 170B color. RS 422/485 RS 232 RS 232 IF 1B IF 1A IF 2 (PLC) (PLC) (PRINTER/DOWNLOAD) |
2/16/2012 1:34 PM | |
Posts: 11 Rating:
|
Tank you very much! |
Follow us on