3/21/2013 8:17 PM | |
Joined: 1/28/2009 Last visit: 3/29/2025 Posts: 6867 Rating:
|
Hello, Communication from S7 300 to a micro controller on physical layer of RS485 may include PROFIBUS or MODBUS.For S7 300, there are some communication processors or integral facility to established mentioned communication protocols with communication partners.If you are using those standard protocols , you can find programming functions in STEP7.For MODBUS,You need to install point to point communication packages or MODBUS master and SLAVE packages. The big problem would be in microcontrollers' side.You should define the response data frames in a determined time.You can also check this website: http://www.hms.se/products/abic.shtml Best regards ![]() Hamid Hosseini |
Follow us on