11/24/2018 8:19 AM | |
Posts: 2 Rating:
|
Hi there, I have an Windows10 -PC with 64 Bit. The S7 Software is not running on this PC. The comunication is between Simatic pc adapter usb a2 (series. 6GK1 XXXXXXXX) over Prodave MPI, to the PLC. At the installation of driver from CD V1.0, there is no failure. I have tried several drivers, but no one is running. I´ll be very lucky when some can give me a solution. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Newcomer-Siemens2018 at: 11/24/2018 12:16:21 PMHello is there someone outside, or I´m alone with my question... Last edited by: Jen_Moderator at: 11/24/2018 7:44:37 PMNew subject after splitting |
|
11/26/2018 10:23 AM | |
Joined: 8/3/2009 Last visit: 3/21/2025 Posts: 15056 Rating:
|
Hello I think the PC Adapter Driver 1.0 is not supportet for Win10 only up to win7. Perhaps you need a newer Diver -> do you have a current Simatic Net PC Software DVD, Just do install to get the latest drivers... Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on