1/30/2015 10:36 AM | |
Posts: 9 Rating:
|
Dear All, I have a Profibus PA / Foundation Fieldbus transmitter : http://www.prelectronics.com/pdf/5350A-2201-US.pdf and a DP/PA coupler Ex [ia]: I config DP/PA coupler Ex [ia] in Step 7 simatic but I don’t see Hardware in “HW Config” of Step 7. Then I don’t config for it. Can you help me connect two device via Profibus PA? Thanks for All.. |
Last edited by: Min_Moderator at: 1/30/2015 11:22 AMEdit link to permanent Last edited by: AchutVn2T at: 1/30/2015 10:36 AM |
|
1/30/2015 10:49 AM | |
Posts: 11 Rating:
|
Hello AchutVn2T, have a look at this FAQ: http://support.automation.siemens.com/WW/view/en/22729270 Regards |
This contribution was helpful to
1 thankful Users |
1/30/2015 11:07 AM | |
Posts: 9 Rating:
|
DearMichiJay, This link: http://support.automation.siemens.com/WW/view/en/22729270 My problem is no see HW ofDP/PA coupler Ex [ia] (6es7157-0ad82-0xa0) in Step 7. Thanks for replay. |
Last edited by: AchutVn2T at: 1/30/2015 11:14 AM |
|
1/30/2015 4:46 PM | |
Posts: 1058 Rating:
|
Hello AchutVn2T, if you dont see HW of DP/PA coupler in your HW catalog, download the GSD file for it and install in HW catalog. You will find GSD file of your coupler here: PROFIBUS GSD files : LINK If you use external master you might also need this: How do you connect the IM 157/IM 153-2 in the DP/PA Link to an external master or a SIMATIC S5? (GSD tool) regards |
This contribution was helpful to
1 thankful Users |
1/31/2015 2:23 AM | |
Posts: 9 Rating:
|
Thanks your answer, I will check again and report for all. |
4/17/2015 12:41 PM | |
Posts: 9 Rating:
|
Dear all, Come back to my project. Now, I still don't connect PR 5350 to PLC CPU314 2PN/DP via DP/PA coupler (157-0AD82-0XA0). I thing have two reson: - DP/PA coupler (157-0AD82-0XA0) can't conect to PR 5350 (Profibus PA). Or - PR 5350 wrong in hardware. If you did same my project, could you help me? Thanks for all! AttachmentImage.rar (81 Downloads) |
Last edited by: AchutVn2T at: 4/17/2015 1:24:22 PM |
|
4/20/2015 12:01 PM | |
Posts: 9 Rating:
|
Can you check my information in attach file and help me? I very worry |
Follow us on