6/27/2011 7:53 AM | |
Joined: 3/21/2006 Last visit: 3/14/2025 Posts: 10239 Rating:
|
Hello, For example, you could use http://support.automation.siemens.com/WW/view/en/29737950 Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
6/27/2011 9:50 AM | |
Joined: 10/7/2005 Last visit: 3/17/2025 Posts: 3042 Rating:
|
Hello niila Allow me to suggest you have a look at using S7 communications instead of the OpenIE ones as you may find them easier to use. The link below contains plenty of examples, if your data volume is less than 160 bytes, GET/PUT will do the job, ifits more then I would opt for BSEND/BRECV. S7-300 CPU 31x -- Configuring and programming communication -- Using communication blocks Additional examples can also be found at Simatic Net quickstart page. If you really want to use the OpenIE ones, I suggest youuse at leastan ISO-on-TCP link instead of pure TCP and you'll find an awful lot of good reference info in the Compedium below: CPU-CPU communication with SIMATIC controllers (compendium) I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on