2/20/2015 9:19 PM | |
Posts: 27 Rating:
|
Hi, Working with a 417-4 cpu Simatic PCS7 V7.1 SP1 I will install a profibus card to communicate between our PLC and an other PLC. https://www.br-automation.com/en/products/networks-and-fieldbus-modules/profibus-dp/3if7629/ I did install the GSD file into my hardware. I have this interface list (see reg.jpg attachement). In the interface list, I can read Send Data Data length: 120 Words (240 Byte = modul_64e + 64e + 64e + 32e + 10e + 2e + 2e + 2e) Receive Data Data length: 16 Words (32 Byte = modul_32a) I did add the modules in the same order that mention into the interfacelist I have. (see cardconfig.jpg) How do I know it will read into the interfacelist as I want? Slot1 read DW1 to DW 32 (64 bytes, modul_64e) Slot2 read DW32 to DW64 (64 bytes, modul_64e) Slott3 read DW64 to DW96 (64 bytes, modul_64e) Slot4 read DW96 to DW112 (32 bytes, modul_32e) Slot5 read DW112 to DW117 (10 bytes, modul_10e) Slott6 read DW118 (2 bytes, modul_32e) Slot7 read DW119 (2 bytes, modul_64e) Slot8 read DW120 (2 bytes, modul_64e) Slot9 read DW1 to DW32 (32 bytes, modul_32a) Thank to help me!! Attachmentcardconfig.zip (116 Downloads) |
2/5/2018 11:10 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by ahmaddedi22 is split to a separate thread with the subject What to set user_prm_Data (3 to 4) under parameter assaigment in hardware configuration?. Best regards |
Follow us on