9/16/2008 10:39 PM | |
Posts: 487 Rating:
|
Hi, You can also extend the length without repeater by using extension plug at the end. This is a newer product but really useful. Please check the link below. https://mall.automation.siemens.com/DE/guest/index.asp?aktprim=0&lang=en&nodeID=10023950&foldersopen=-4287-4288-4633-4755-4757-&jumpto=4757 |
9/16/2008 11:08 PM | |
Posts: 487 Rating:
|
I think it will support 62X2=124 slaves. The following section is taken from the module manual.
It is clearly mentioning A&B slaves for both masters of a dual master. Here is another quote from the manual.
Check the link below from A&D Mall Dual Master Here it clearly says
So I think it is pretty clear that it supports 62 X 2 |
9/17/2008 7:43 PM | |
Posts: 196 Rating:
|
Hi JMJ Thanks for all the information. |
Follow us on