1/1/2020 7:39 AM | |
Joined: 11/15/2015 Last visit: 1/31/2025 Posts: 179 Rating:
|
Dear JKV JAMES Good morning all Make a logic in the PLC program that when the button is pressed >>>>> then make the timer on/of ,on/off followed by an up counter >>>>> then your value will add depending on the number of pulses you can configure your function according to your requirements. Regards, |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
This contribution was helpful to
2 thankful Users |
Follow us on